SLUUD41A August 2024 – November 2024 TPSM82843
The output voltage can be adjusted through the choice of Rx1 and Rx2/Rx3 resistors. Since Rx1 and Rx2/Rx3 are in parallel, only Rx1 or Rx2/Rx3 must be installed one at a time. Rx1 is an 0402 size to represent a typical device in an actual application. However, such a small size is difficult to replace. Therefore, Rx2/Rx3 is provided in an 0603 size to change the output voltage easily. Simply remove Rx1 and place the desired value to Rx2/Rx3. The required resistor for the target output votage selction is listed in a table in the data sheet.