SLUUD46 October 2024 BQ25188
To go to Ship Mode, enable ship mode through an I2C transaction to set EN_SHIP_RST bits or the PB_LPRESS_ACTION bits as shown in Figure 2-6:
Enter Ship mode by removing VIN if setting EN_RST_SHIP to 2b01. If setting PB_LPRESS_ACTION to 2b10 to enable Ship mode, then hold the TS/MR button for the configured tLPRESS then remove VIN.
When the voltage on the SYS (SC#2) falls to 0V, Ship mode has been enabled.