SLUUD47 October 2024 BQ21088
Connect the equipment as the following:
Turn the supply PS#2 on, then turn the supply PS#1 on. The VSYS rises to 4.5V. The device begins to charge as long as the TS is left at default configuration and there are no other faults.
To adjust the charge current or change other parameters, connect the USB2ANY to the EVM and then start up the TI Charger GUI.
Select the BQ2518X from the charger selection. Click Quick Start or Register Map.
The Quick Start is shown in Figure 2-4.
The register map is shown in Figure 2-5.