SLUUD47 October 2024 BQ21088
The BQ21088EVM is an evaluation kit for the BQ21088 integrated battery charge management IC. The BQ21088 is an integrated battery charge management IC that integrates the most common functions for wearable devices: linear charger, regulated output, manual reset with timer, and ship mode function. The low quiescent current (IQ) during operation and shutdown enables maximum battery life.
This user's guide provides detailed testing instructions for the BQ21088 evaluation module (EVM). Also included are descriptions of the necessary equipment, equipment setup, procedures, the printed-circuit board layouts, schematics, and the bill of materials (BOM). Throughout this user's guide, the abbreviation EVM, BQ21088EVM, and the term evaluation module are synonymous with the BQ21088 evaluation module, unless otherwise noted.
![]() |
|
Hot surface! Contact can cause burns. Do not touch! Some components can reach high temperatures >55°C when the board is powered on. The user must not touch the board at any point during operation or immediately after operating, as high temperatures can be present. |