SLUUD53 September 2024 TPS51388
The schematic for the TPS51388EVM is shown in Figure 4-1.
The default operating frequency of TPS51388EVM is 600kHz. If the user wants to test the device behavior at 1000kHz (typical value), please use the jumper to short MODE to GND.
BYP pin is an external 5V VCC input and can connect to the output of the buck regulator if the output voltage is set between 4.8V to 5.2V. In the TPS51388EVM, since the output voltage is 5.15V, connect BYP to the output voltage through JP5. If the output voltage is less than 4.8V and the user wants to improve the light load efficiency, then remove the jumper on JP5, and the external BYP voltage is higher than 4.8V. Note that the BYP external voltage must come after VIN voltage on and quit before VIN off.