Flashing FW on initial units.
- Download and install
BQstudio, BQstudio appears as BatteryManagementStudio in the computers
directory.
- Inside the BatteryManagementStudio folder there is a folder labeled
"config". Place the "4190_0_01-bq41z90.bqz" file inside the config
folder.
- Connect the communication
cable to the SMBus port on the EV2400 and J7 on the BQ41z90EVM. The Jumpers
on J28 and J29 need to be uninstalled.
- Launch BQstudio, the device
does not automatically detect. Force open the 4190_0_01-bq41z90.bqz by
selecting gauges and then selecting 4190_0_01-bq41z90.bqz and pressing
Finish. A warning appears, press "ok".
- Go to the "Programming" tab on BQstudio, select
"bq41z90_v0_01_build_1.sig.enc.bq.fs" and press program.
- The device is now programmed
with the BQ41z90FW, the next time BQstudio is opened the device is
automatically detected.
Find the latest firmware version in the appropriate BQ41Z90 folder on www.ti.com. Use the following steps to install the BQ41Z90 Battery Management Studio software:
- Run Battery Management Studio from the
Start > Programs > Texas Instruments > Battery
Management Studio menu sequence, or the Battery Management Studio
shortcut.
- Follow the directions in Programming Screen, select the firmware .bq.fs file downloaded from www.ti.com, and click the Program button.
- Once programming is finished, the EVM is ready to use with the latest firmware.