SLUUD69 December 2024 TPS923650
PRODUCTION DATA
The EVM can be set up in both Boost connection and Buck-Boost connection.
For Boost connection, connect the output of the input power supply to the J1 terminal block. Connect the LED load to the J3 terminal block. Pay attention to the polarity of the LED load. Connect the output of the function generator to the TP6 (positive) and TP3 (negative). As an example, Figure 2-1 shows the connection diagram of TPS923651D1DSGREVM in Boost connection. For other EVMs for WSON package and HVSSOP package, the connection should be done in the same way. For EVMs for SOT583 package, the layout is mirrored to the EVMs for WSON package and HVSSOP package. As an example, Figure 2-2 shows the connection diagram of TPS923650D1DRLREVM in Boost connection. For TPS923650D2DRLREVM, the connection should be done in the same way.
For Buck-Boost connection, connect the output of the input power supply to the J1 terminal block. Connect the LED load to the J2 terminal block. Pay attention to the polarity of the LED load. Connect the output of the function generator to the TP6 (positive) and TP3 (negative). As an example, Figure 2-3 shows the connection diagram of TPS923651D1DSGREVM in Buck-Boost connection. For other EVMs for WSON package and HVSSOP package, the connection should be done in the same way. For EVMs for SOT583 package, the layout is mirrored to the EVMs for WSON package and HVSSOP package. As an example, Figure 2-4 shows the connection diagram of TPS923650D1DRLREVM in Boost connection. For TPS923650D2DRLREVM, the connection should be done in the same way.