SLUUD71 December 2024 TPS922051
PRODUCTION DATA
The EVM can be set up in the below way.
Connect the output of the input power supply to the J1 terminal block. Connect the LED load to the J2 terminal block. Pay attention to the polarity of the LED load. Connect the output of the function generator to the TP5 (positive) and TP2 (negative). As an example, Figure 2-1 shows the connection diagram of TPS922051D1DSGREVM. For other EVMs for WSON package and HVSSOP package, the connection should be done in the same way. For EVMs for SOT583 package, the layout is mirrored to the EVMs for WSON package and HVSSOP package. As an example, Figure 2-2 shows the connection diagram of TPS922050D1DRLREVM. For TPS922050D2DRLREVM, the connection should be done in the same way.