SLVA275C january 2010 – may 2023 UCD9081
The SaveRailLog field in the configuration parameters specifies whether each rail is marked to write the error log to flash upon rail failure. If the rail is marked this way, then a shutdown of this rail is logged info non-volatile memory. In this case, the NVERRLOG bit (STATUS register) is set to 1 upon device initialization and must be cleared before normal sequencer operation is restored. See the section titled Resetting the Flash Error Logs for detailed instructions.
The contents of this register are as follows:
The default value for this register is 0x0000.