SLVA528D September 2012 – August 2021 TPS65381-Q1 , TPS65381A-Q1
C2000 and Hercules, are trademarks of Texas Instruments.
All trademarks are the property of their respective owners.
The system and equipment manufacturer or designer (as user of this document) is responsible to ensure that their systems (and any TI hardware or software components incorporated in their systems) meet all applicable safety, regulatory, and system-level performance requirements. All application and safety-related information in this document (including application descriptions, suggested safety measures, suggested TI products, and other materials) is provided for reference only. Users understand and agree that their use of TI components in safety-critical applications is entirely at their risk, and that user (as buyer) agrees to defend, indemnify, and hold harmless TI from any and all damages, claims, suits, or expense resulting from such use.
This safety manual provides information to help system developers create safety-related systems using the supported TPS65381x-Q1 multirail power supply. This document contains:
Separate documents provide the following information, not covered in this document:
TI expects that the user of this document has a general familiarity with the TPS65381x-Q1 device. This document is intended to be used in conjunction with the pertinent data sheets and other documentation for the products under development. This partition of technical content is intended to simplify development, reduce duplication of content, and avoid confusion as compared to the definition of safety manual in IEC 61508:2010.
The TPS65381x-Q1 device is a multirail power supply designed to supply microcontrollers (MCUs) in safety-relevant applications, such as those found in automotive and industrial markets. The device supports Texas Instruments’ Hercules™ TMS570 MCU and C2000™ families, and various other MCUs with dual-core lockstep (LS) or loosely-coupled architectures (LC).
The TPS65381x-Q1 integrates multiple supply rails to power the MCU, transceiver (CAN or other), and an external sensor. An asynchronous buck switch-mode power-supply converter with internal FET converts the input supply (battery) to a 6-V preregulator output. This 6 V supplies the other regulators.
The integrated 5-V linear regulator with internal FET is typically used to supply a transceiver or other peripheral. A second integrated linear regulator, also with internal FET, regulates to a selectable 5-V or 3.3-V MCU I/O voltage.
The TPS65381x-Q1 includes the VDD1 voltage-regulator controller, typically used to supply the MCU core rail. This linear regulator controller uses an external FET and resistor divider (for adjustment). It regulates the 6 V to an adjustable voltage of between 0.8 V and 3.3 V for the core.
The device includes a sensor supply, VSOUT1.
The device has an integrated charge pump to provide an overdrive voltage for the internal regulators. One option for reverse-battery protection uses the charge-pump output to control an external NMOS transistor. This solution allows for a lower minimum battery voltage operation compared to a traditional reverse-battery blocking diode because there is less voltage drop across the transistor.
The device monitors undervoltage and overvoltage on all regulator outputs, battery voltage, and internal supply rails. A second band-gap reference, independent from the main band-gap reference, monitors for undervoltage and overvoltage, to avoid any drifts in the main band-gap reference being undetected. In addition, the device implements regulator current limits and temperature protections.
The TPS65381x-Q1 functional safety architecture features a watchdog configurable for question and answer (Q&A) mode or trigger mode, MCU error-signal monitor (ESM), diagnostic check for the MCU ESM, clock monitoring on internal oscillators, self-check on clock monitor, CRC on internal nonvolatile memory (EEPROM), CRC for configuration registers, diagnostic multiplex output to route internal analog (AMUX) and digital (DMUX) signals out through the DIAG_OUT pin, and a reset circuit for the MCU. A built-in self-test (BIST) allows for monitoring the device functionality at power up.