SLVAE32B August   2018  – December 2023 TPS7H2201-SP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Device Overview
  5. Single-Event Effects
  6. Test Device and Evaluation Board Information
  7. Depth, Range, and LETEFF Calculation
  8. Irradiation Facility and Setup
  9. Test Setup and Procedures
  10. Single-Event-Latchup (SEL), Single-Event-Burnout (SEB), and Single-Event-Gate-Rupture (SEGR)
    1. 7.1 Single-Event-Latchup (SEL)
    2. 7.2 Single-Event-Burnout (SEB) and Single-Event-Gate-Rupture (SEGR)
  11. Single Event Transient (SET)
  12. Total Ionizing Dose From SEE Experiments
  13. 10Orbital Environment Estimations
  14. 11Confidence Interval Calculations
    1. 11.1 Rate Orbit Calculation
  15. 12Summary
  16. 13References
  17. 14Revision History

Single-Event-Latchup (SEL)

All SEL characterizations were performed with die temperature of 125°C. The device was heated by connecting three parallel power resistors (model: RP60800R0100JNBK) attached with thermal paste to the back of the board. The temperature was monitored by attaching a K-type thermocouple to the thermal pad of the device on the top layer. Thermocouple and die correlation was verified by using a thermal IR camera, prior to reach to the heavy-ions facility (TAMU).

The device was exposed to a Praseodymium (Pr) heavy-ion beam incident on the die surface at 0° and 27.3° for an LETEFF of 66.43 and 75 MeV-cm2 / mg, respectively. Flux of approximately 105 ions / cm2 × s and fluence ≥ 107 ions / cm2 was used in each run. Run duration to achieve this fluence was approximately two minutes (for 107 ions / cm2). During the SEL testing, the device was set up as described in Figure 3-3. Table 7-1 summarizes the SEL results. No SEL events were observed under any of the test runs, indicating that the TPS7H2201-SP is SEL-immune at T = 125°C and LET = 75 MeV·cm2 / mg. SEL cross-section was calculated based on 0 events observed using a 95% (2σ) confidence interval (see Section 11 for discussion of cross-section calculation method). Figure 7-1 shows a typical current plot.

Equation 1. σ S E L 1.84 × 10 - 7 c m 2 / d e v i c e   f o r   L E T E F F = 75 M e V × c m 2 / m g   a n d   T J = 1 25 ° C ,   95 %   c o n f .
Table 7-1 Summary of TPS7H2201-SP SEL Results With T = 125°C and LETEFF = 74.83 MeV-cm2/ mg
Run NumberUnit NumberTemperature (°C)Ion TypeAngle of Incidence (°)LETEFF (MeV × cm² / mg)Flux (ions / cm² × s)Fluence (ions / cm²)VIN (V)Load (A)SEL Events
11125Pr27.3751.07 × 1052 × 107760
21125Pr066.431.14 × 1059.95 × 106760
GUID-DC89517E-B4A5-4601-8857-F45138CD0A3F-low.gifFigure 7-1 Current Versus Time for SEL Run 1 at T = 125°C and 75 MeV × cm2/ mg