SLVAEK2A December   2019  â€“ December 2020 TPS2H160-Q1

 

  1.   Trademarks
  2. 1Overview
  3. 2Functional Safety Failure In Time (FIT) Rates
  4. 3Failure Mode Distribution (FMD)
  5. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a Failure Mode Analysis (FMA) for the pins of the TPS2H160-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to Ground (see Table 4-2)
  • Pin open-circuited (see Table 4-3)
  • Pin short-circuited to an adjacent pin (see Table 4-4)
  • Pin short-circuited to supply

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
Class Failure Effects
A Potential device damage that affects functionality
B No device damage, but loss of functionality
C No device damage, but performance degradation
D No device damage, no impact to functionality or performance

Figure 4-1 shows the TPS2H160-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TPS2H160-Q1 data sheet.

GUID-20201202-CA0I-M57F-KP8Q-LLCFCLBBH5QJ-low.png GUID-20201202-CA0I-0F0D-LMXW-4T5FGF7K04JZ-low.png Figure 4-1 Pin Diagram
The pin FMA is provided under the assumption that the device is operating under the specified ranges within the Recommended Operating Conditions section of the data sheet.
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
INx 1,2 Shutdown of corresponding channel B
DIAG_EN 3 Diagnostics will be disabled B
NC 4,10 Pin 4 is NC for Version A only. No effect D
FAULT 4 Version B only: Fault status reported may be erroneous B
STx 5,6 Version A only: Status being reported may be erroneous B
SEL 5 Version B only: If DIAG_EN is high then channel 1's sense current output always on SNS B
CS 6 Version B only: Sense current not valid from CS pin B
CL 7 Device will default to internal current limit C
GND 8 Resistor/diode network will be bypassed if present B
THER 9 Device will default to "auto-retry" mode when encountering thermal fault B
OUTx 11,12,15,16 Current limit of device will engage B
VS 13,14 Device will have no input supply and therefore not function B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
INx 1,2 Corresponding channel will be shutdown and INx will be pulled down internally B
DIAG_EN 3 Diagnostics will be disabled with device as pin will be pulled down internally B
NC 4,10 Pin 4 is NC for Version A only. No effect D
FAULT 4 Version B only: Fault signal not reported B
STx 5,6 Version A only: STx pin cannot pull high and diagnostics cannot be reported B
SEL 5 Version B only: Pin pulled low internally, however wrong SNS current potentially reported on CS if DIAG_EN is high B
CS 6 Correct CS current cannot be read B
CL 7 Channel 1 and 2 will not be able to provide output current B
GND 8 Loss of ground detection engages and device shuts off B
THER 9 Internally pulled down and device will default to "auto-retry" mode when encountering thermal fault B
OUTx 11,12,15,16 No effect. If configured, open load detection will trigger B
VS 13,14 Device will have no input supply and therefore not function B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effect(s) Failure Effect Class
IN1 1 IN2 IN1 signal will affect IN2 signal and vice versa B
IN2 2 DIAG_EN IN2 signal will affect DIAG_EN signal and vice versa B
DIAG_EN 3 NC Version A only. No effect D
DIAG_EN 3 FAULT Version B only. Signal of DIAG_EN could affect FAULT signal and vice versa B
NC 4 ST1 Version A only. No effect D
FAULT 4 SEL Version B only. FAULT status could affect SEL signal and vice versa B
ST1 5 ST2 Version A only. False ST1 status could be reported on ST2 and vice versa B
SEL 5 CS Version B only. Signal on SEL could affect signal on CS pin and vice versa B
ST2 6 CL Version A only. If ST2 is high then and channel 1 and channel 2 will not be able to provide output current. If ST2 is low the internal current limit will be set B
CS 6 CL Version B only. Voltage level on CS could cause erroneous current limit to be set on device B
CL 7 GND Device will default to internal current limit B
THER 9 NC No effect D
NC 10 OUT2 No effect D
OUT2 11 OUT2 No effect D
VS 13 VS No effect D
VSx 12,15 VOUTx Output will be pulled supply voltage. Short-to-battery detection will be triggered if configured B
OUT1 15 OUT1 No effect D
Table 4-5 Pin FMA for Device Pins Short-Circuited to supply
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
INx 1,2 Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell A
DIAG_EN 3 Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell A
NC 4,10 Pin 4 is NC on Version A only. Pins not internally connected D
FAULT 4 Version B only. Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell A
SEL 5 Version B only. Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell A
STx 5,6 Version A only: Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell A
CS 6 Version B only: Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell A
CL 7 Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell A
GND 8 Supply power will be bypassed and device will not turn on B
THER 9 Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell A
OUTx 11,12,15,16 Output will be pulled supply voltage. Short-to-battery detection will be triggered if configured B