SLVAET3 October 2021 TPS8802
All of the identified sources of current consumption are tabulated in a spreadsheet to calculate the system power consumption. The spreadsheet uses a set of system parameters and measurement subroutines to break down the power consumption block-by-block for each measurement subroutine. The decomposition allows users to identify the biggest sources of power consumption when testing their system and further reduce the system power.
The power calculation is based on the schematics in Section 2.5. These schematics and associated power calculation can be modified based on the system requirements. One of the key calculation parameters is that the IR LED is the primary method of smoke detection. When the smoke concentration is low, the IR LED is used to measure the smoke level. When the smoke concentration rises, the IR and blue LED are used to measure the smoke level. Because only the IR LED is pulsed most of the time, only the IR LED power consumption is considered.