USB Type-C interface is quickly becoming one of the most popular ways of connecting electronic devices. From speakers to laptops, a single USB Type-C port can deliver power and offer high-speed data transfer. However, USB Type-C faces its own set of design challenges such as the process of Fast Role Swap (FRS). Its power-protection devices also need to qualify for the unique design specifications while protecting the port from overvoltage, short circuit, and reverse current. The TPS25947 efuse and LM73100 ideal diode can offer power protection while meeting the USB-Type C requirements for robust high power delivery, high-speed data transfer, and FRS.
Figure 1-1 shows that two protections devices are needed per port to protect the system at all times especially during FRS.
Fast Role Swap (FRS) Explained
FRS describes the process when the device transitions from a power sink to a power source and vice versa. A laptop docking station, for example, requires robust FRS design and protection to ensure uninterrupted power supply to its accessories when external power disconnects. To further put FRS into perspective, imagine the setup in Figure 2-1: a laptop and its docking station connected through a single USB Type-C. The docking station initially charges the laptop and powers the other accessories through external power source. When the external power is removed, the laptop needs to quickly transition from a power sink to a power source to continuously supply power for its connected accessories. There are two major challenges in FRS:
While meeting FRS requirements with fast charging and linear ORing, TPS25947 and LM73100 also feature adjustable overvoltage and undervoltage protection that ensures a smooth FRS within the 5-V specification.
For this test in Figure 3-1, Vout was initially supplied at 20 V by an external source, indicating that the end device is initially a power sink. Once the external supply is disconnected, Vout quickly drops and the end device switches to a power source to match a constant 5-V output. As shown by Figure 3-1, TPS25947 is able to FRS in ~30 µs.
When multiple USB Type-C ports could supply or receive power, robust RCB is required to prevent current leakage between adjacent ports as shown in Figure 4-1. Without RCB, any buildup of reverse current leakge could cause permanent damage to the entire system. A typical slow ramp-up test can identify current leakage. If present, increasing the power on one port would charge up the adjacent port.
RCB is implemented using back-to-back FETs. Shown in Figure 4-2, switching off the blocking FET allows the device to block reverse current from output to input.
Conventionally, a comparator controls the switching of the FET for RCB. Reverse current is allowed to build up as long as the current does not exceed the comparator threshold. Linear ORing provides true RCB by adjusting the resistance of the blocking FET to maintain a constant voltage across it. If forward current is increasing, the resistance of the blocking FET is reduced. If forward current is decreasing, the resistance of the blocking FET is increased, eventually shutting off the blocking FET before reverse conduction occurs. Linear ORing forces the device to go from forward conduction to a 0 point without allowing reverse conduction to ever occur.