Choose R2 so that the current flowing through the
feedback network is approximately 1 mA.
Choose R3 to set the output voltage to the
desired value.
Choose a product of output capacitance
CO and equivalent series resistance RESR to generate a zero below
10 kHz (lower is generally better). The frequency of the ESR zero is given
by:
RESR can
be either inherent in the capacitor used or included separately in series with a low-ESR
capacitor (as it was in this case).
An optional feedforward capacitor CFF across the feedback network provides an
additional zero that improves transient response. The value of CFF is best
selected experimentally. Note that CFF cannot be used on its own to stabilize
the loop. This is because the pole and the zero formed by R2, R3, and CFF are
too close to each other in the frequency domain to stabilize the loop over the whole range
of output currents.
An additional capacitor, C1, reduces the initial voltage step response caused by the relatively
high value of RESR. The value of C1 is low
compared to CO and does not significantly affect stability.