All trademarks are the property of their respective owners.
While the active clamp forward topology enables high efficiencies for PoE DC/DC designs, there are certain design considerations or component selections that require special attention. One such consideration is the stress on the switching MOSFETs. When power is removed, the behavior of the controller can create situations that cause either high voltage or high current in the circuit (or both).
To address this condition, one approach is to increase the ratings of parts (example: a higher voltage MOSFET). While this quickly solves the problem with little design effort, this approach leads to higher system cost. As the output voltage of the DC/DC converter increases, the stress on the MOSFETs increases, driving the cost up disproportionately to the output voltage increase. Since the voltage and current spikes are not the nominal values of the switching voltages and currents, the opportunity for lower cost parts is possible if the spikes are addressed in another way. This will also drive the cost ramp down for higher output voltage active clamp forward designs.
The TPS23730, TPS23734, and TPS23734 devices introduce a new approach, called soft-stop. This approach consists of controlling the discharge of the output capacitor of the converter, and subsequently sending the energy back to the input bulk capacitor.
Figure 1-1 illustrates an active clamp forward design.
When the input power is removed, the input voltage rails gradually decrease as the input bulk capacitor is discharged. The converter will remain on as the input voltage decreases to its minimum threshold. As the input voltage decreases, the converter increases the duty cycle to compensate. This leads to shorter and shorter off times, and the voltage across the clamp capacitor approaches higher values since the transformer is being reset so quickly. The end result is oscillations and overvoltages that could potentially damage the MOSFETs. Figure 2-1 illustrates these principles.
Additionally problematic, if a brief power interruption occurs during the next power up, the clamp capacitor will be precharged, which could cause the transformer to saturate. This causes severe stress on the switching components. In this case, the N-FET on the primary side of the transformer and the secondary sync FET (Q3) are at risk. This is explained in more detail in the Line Undervoltage Protection section of the UCC2897A Advanced Current-Mode Active-Clamp PWM Controller Data Sheet.
Another case during shutdown is when the converter stops prematurely because the controller has an undervoltage lockout (UVLO). If this threshold is reached when the output voltage is too high, the risk of “backdrive” becomes possible. Backdrive is when the output voltage is high enough to turn on the MOSFET on the secondary side, and this results in energy being driven from the secondary to the primary. The output voltage turns on the gates of both secondary MOSFETs, not at the same time but they eventually are both ON at the same time. Since both MOSFETs are ON, there is approximately 0 V across the transformer secondary inductance.
There are now two current paths on the output. The total VOUT discharge current builds up in the inductance, and a fraction of the discharge current flows through the magnetizing inductance of the transformer. After a short time, the inductor current becomes very high. Over time, the output voltage is dropping so both ends of the secondary goes down. This leads to both MOSFETs turning off. However, the transformer magnetizing current has to be maintained, so it gets transferred to the primary side. This is possible because the series synchronous MOSFET (Q5) is turning off, generating a reverse polarity on the transformer. This forces current through the primary clamp capacitor, and also consequentially, this turns on the parallel synchronous MOSFET (Q3).
This pattern continues until the energy in the circuit is too low to turn on the MOSFETs. In this case, the design may require a 200-V (instead of 150 V) rating with avalanche rating for the N-FET and ≥ 100 V (instead of 60 V) (example: 12-V application) rating for Q5 (in Figure 1-1). This is higher BOM cost. The soft-stop feature reduces or eliminates these spikes, thus leading to lower BOM cost.