SLVAF18 March 2021 TPSM5601R5H
We tend to associate EMI with wireless interference but there is also an interference that travels through a conducted path instead of the air. Conducted EMI is a form of conduction coupling generated via cabling, PCB traces, parasitic elements, or power and ground planes. Radiated EMI is the coupling of unwanted signals from radio transmissions due to the elements of conducting materials. Every conductor has characteristics of an antenna that is capable of both transmitting and receiving signals.