SLVAF38 March 2021 TPS61096A
In some special application scenarios of boost converters, the output voltage required by the customer could be up to 150 V, which is much higher than the capability of a general boost converter. Taking TPS61096A as an example, its maximum output voltage is only 28 V because of the voltage limitation of the integrated power switch. This application note introduces a method of using a coupled transformer to increase the output voltage level of the boost converter.