SLVAFC5 March 2022 TPS629210 , TPS629210-Q1
The input voltage that can be applied to an inverting buck - boost converter is less than the input voltage that can be applied to the same buck converter. This is because the ground pin of the IC is connected to the negative output voltage. Therefore, the input voltage across the device is VIN to -VOUT, not VIN to ground. Thus, the input voltage range of the TPS629210-Q1 is 3 V + VOUT to 17 V+ VOUT, where VOUT is a negative value.
The output voltage range is the same as when configured as a buck converter, but negative. The TPS629210-Q1 output voltage for the inverting buck - boost topology should be set between –0.6 V to –5.5 V for external divider and -0.4 V to -5.5V for internal divider (VSET). It can be set the same way as in the buck configuration, with two resistors connected to the FB pin or VSET configuration. Due to the increased noise of the inverting buck - boost topology, for a more robust design, recommend use internal feedback (VSET) or use smaller value resistors than are used for the buck configuration.