SLVAFC9 August 2022 TPS61094
An energy storage element is a necessary condition to realize this system, Supercap or batteries can be used here as energy storage elements. For this system, the capacity of the energy storage element needs to meet the power supply requirements of the system during the dark hours of the day. The choice of the supercap or batteries can be calculated by the following equation.
Here select, η≈90%, according to the environment condition and system requirement. The supercap needs to be able to discharge at a constant power of 1 mA for 12 hours. Based on Equation 1, the super cap in the system needs to be more than 55 F.