SLVAFE4 june   2023 TLC6983

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Common issues in NPP Matrix LED Panel
    1. 2.1 Ghosting
    2. 2.2 Non-Uniformity in Low Gray Scale
    3. 2.3 Coupling
    4. 2.4 Caterpillar
    5. 2.5 Color Shift in Low Gray Scale
    6. 2.6 Gray Scale Gradient Discontinuity Issue
    7. 2.7 First Scan Line Dim
  6. 3Summary
  7. 4References

First Scan Line Dim

Figure 2-15 shows the first scan line dim issue. In ultra-low illumination the first line of each stackable led matrix will darker than other lines. The voltage of un-conducted line is forced to float with the turn-on OUTx. Since the uncertainly starting voltage of first line, whose voltage can be higher or lower than other lines, causing the first line of every multiplexing is darker comparing to other lines.

GUID-20220628-SS0I-WMQW-QDH1-QBQVW8Z5QG0V-low.gif Figure 2-15 First Line Dim Issue