SLVAFE9 September 2022 AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442 , TPS65219 , TPS65220
Use case: VSYS=3.3V, LDDR4 Memory
Figure 4-7 shows the TPS6521902 variant powering the AM64x processor on a system with 3.3 V input supply and LDDR4 memory. Buck1, LDO3, LDO2, and LDO1 are used to supply the same AM64x domains that were described in the previous block diagram. The 3.3 V coming from the pre-regulator can be combined with a power switch to supply the 3.3 V VDDSHVx IO domain. The GPO2 is pre-programmed to be enabled in the second slot of the power-up sequence with a duration of 10ms. It can be used to enable the external power switch and meet the processor sequence requirements. The switch must be selected with the right electrical spec to ramp and provide a stable output voltage within the 10 ms duration of the second slot (before the PMIC starts the next slot in the power-up sequence). Buck3 and Buck2 supports the 1.1 V and 1.8 V required by VDDS_DDR and the 1.8 V DVDD3V3 IO domain. They are also used to support the required voltages on the LPDDR4 memory. LDO4 is a free 2.5 V power resource that can be used for external peripherals like the Ethernet PHY. GPIO and GPO1 are free digital resources that are disable by default but could be enabled through I2C if needed. Figure 4-8 and shows the power-up and power-down sequence programmed on TPS6521902.