The following is the flow diagram detailing the process for burst mode download.
Figure 4-5 shows the process for burst mode download. After the host confirms that the device has
entered PTCH mode, the host shall implement the sequence below to download the patch
bundle:
- The host initializes the firmware in
preparation for a PBMx load sequence and what the patch bundle contains by writing
6 bytes of data to the DATAx (0x09 if using I2C1 or 0x11 if using I2C2) register:
- 0x06 is first transmitted to tell the
PD controller a 6-byte payload is written.
- Bytes 0 to 3 are the patch bundle
size. In Figure 4-6, the patch bundle size is 0x3500 or 13568 bytes. Byte 4 is the DATAx.SlaveAddress
you want to assign for data transmission. 0x00 or the device's I2C slave addresses
(0x22/0x26 or 0x23/0x27) of the PD controller are not valid. Figure 4-6 shows a random address, 0x35, was selected and used.
- Byte 5 is the burst mode timeout
value (LSB of 100ms). A non-zero value must be used and is recommended to always use
0x32, that gives you a 5 second window to complete the burst mode patch update.
- The host shall start the burst mode patch
download process by sending the 4CC ASCII PBMs task command to the CMDx (0x08 if
using I2C1 or 0x10 if using I2C2) register. 0x04 is first transmitted to tell the PD
controller that a total of 4 bytes will be written.
- Read and poll the CMDx register until
Byte 1 is 0x00, indicating that the task processing is finished.
- Read and poll the DATAx register until
Byte 1 is 0x00, indicating that the patch initialization from step 1 was successful.
- Transmit patch bundle data to the
DATAx.SlaveAddress configured in step 1 in packets of 256 byte. The patch bundle can be
generated as a C style array using the TPS257XX-Q1-GUI (available from v1.2.0). From the BUILD GUI FLASH IMAGE
menu, select SAVE LOW REGION BINARY. Then choose the C Header Source File as the format
and click SAVE. This file will also include the patch bundle size.
- After the patch bundle data is
successfully written, wait 500us and write the PBMc task to the CMDx register to
complete the patch loading sequence. Ensure you are back to writing to the original I2C
slave address of the PD controller from this step.
- Read and poll the CMDx register until
Byte 1 is 0x00, indicating that the task processing is finished.
- Read and poll the DATAx register until
Byte 1 is 0x00, indicating that the device patch bundle download was successful. The I2C
Interrupt, or GPIO9, will be released roughly 110 ms after.
- Write the PBMe task to the CMDx
register to end the patch loading sequence and enter ‘APP’ mode (optional).
- Read the MODE register to check if the
device is in APP mode which indicates that the PD controller received all patch and
application configuration data and is fully functioning in the application firmware.