SLVAFF7B December 2022 – November 2024 TPS25762-Q1 , TPS25763-Q1 , TPS25772-Q1
The firmware patch bundle is used for two purposes:
As described in the previous section, the firmware patch bundle can be loaded from an external EEPROM or from a host after POR by using the device’s I2C host interface. The patch bundle is from a single source. If the configuration and patch data do not load successfully due to communications error, the boot code will use the factory device configurations.