SLVAFF7B December 2022 – November 2024 TPS25762-Q1 , TPS25763-Q1 , TPS25772-Q1
If TVSP is set to external EEPROM patch bundle loading, the device will try to access the address of the external EEPROM (0x50) when powered on. And if an external EEPROM is detected, the boot code firstly attempts to read the patch bundle from the low region of the EEPROM. If any part of the read process yields invalid data, the device aborts the low region read and attempts to read from the high region. If both regions contain an invalid patch bundle, the boot firmware proceeds to enter patch mode. When the device is in patch mode, most features will be limited and only few functions of the device will work. Therefore, the device will enter patch mode when TVSP is set to EEPROM Boot Mode, but is not connected to one.
The device is designed to power the external EEPROM from its internal LDO Regulator LDO_3V3, so pull-up resistors used for the EEPROM memory must be tied to LDO_3V3. Note that the LDO_3V3 can supply external circuits up to 25 mA.
The I2C port supports Standard, Fast Mode, and Fast Mode Plus I2C interfaces. The basic requirements are as below:
Manufacturer | Part Number |
---|---|
On Semi | CAV24C256 |
Microchip | 24LC256 |
ST Micro | M24256 |
Rohm | BRA24T512FVT-3AM |