Part 2 of this topology series discusses how to choose the best-fitting topology from the parameters of the power-supply specification. This application brief describes different in-depth aspects for buck, boost, and buck-boost topologies.
Figure 1-1 shows the schematic of a nonsynchronous buck converter. A buck converter steps down the input voltage to a lower output voltage. The energy transfers to the output when switch Q1 is conducting.
Equation 1 calculates the duty cycle as:
Equation 2 calculates the maximum metal-oxide semiconductor field-effect transistor (MOSFET) stress as:
Equation 3 gives the maximum diode stress as:
where
The bigger the difference between the input voltage and output voltage, the greater the efficiency of the buck converter compared to a linear regulator or low-dropout regulator (LDO).
While a buck converter has a pulsed current at the input, the output current is continuous due to the inductor-capacitor (LC) filter located at the output of the converter. As a result, the voltage ripple reflected to the input is larger compared to the ripple at the output.
For buck converters with a small duty cycle and output currents greater than 3 A, use a synchronous rectifier. If the power supply requires output currents greater than 30 A, use a multiphase or interleaved power stage, because this minimizes the stress for components, spreads the generated heat among multiple power stages, and reduces the reflected ripple at the input of the converter.
Duty-cycle limitations can occur when using an N-FET, because the bootstrap capacitor needs to be recharged every switching cycle. In this case, the maximum duty cycle is in the range of 95%–99%.
Buck converters generally have good dynamic behavior because these converters represent a forward topology. The achievable bandwidth depends on the quality of the error amplifier and the chosen switching frequency.
Figure 1-2 through Figure 1-7 show voltage and current waveforms in continuous conduction mode (CCM) for the FET, diode and inductor in a nonsynchronous buck converter.
A boost converter steps up the input voltage to a larger output voltage. The energy transfers to the output when switch Q1 is not conducting. Figure 1-8 is a schematic of a nonsynchronous boost converter.
Equation 4 calculates the duty cycle as:
Equation 5 calculates the maximum MOSFET stress as:
Equation 6 gives the maximum diode stress as:
where
With a boost converter, a pulsed output current is visible, because the LC filter is located at the input. Thus, the input current is continuous and the output voltage ripple is larger than the input voltage ripple.
When designing a boost converter, it is important to know that there is a permanent connection from the input to the output, even when the converter is not switching. Take precautions in case of a possible short event at the output.
For output currents greater than 4 A, replace the diode with a synchronous rectifier. In case the power-supply needs to provide output currents greater than 10 A, a multiphase or interleaved power-stage approach is recommended.
When operating in CCM, the dynamic behavior of a boost converter is limited due to the right half-plane zero (RHPZ) of the transfer function. Because the RHPZ cannot be compensated, the achievable bandwidth is usually less than one-fifth to one-tenth the RHPZ frequency. See Equation 7:
where
Figure 1-9 through Figure 1-14 show the voltage and current waveforms in CCM for the FET, diode and inductor in a nonsynchronous boost converter.
A buck-boost converter is a combination of a buck and a boost power stage, which share the same inductor (see Figure 1-15).
The buck-boost topology is useful because the input voltage can be smaller, greater, or equal to the output voltage, while the output power needed is bigger than 50 W.
For an output power smaller than 50 W, a single-ended primary inductance converter (SEPIC) is a more cost-effective choice because this converter uses less components.
A buck-boost converter operates in buck mode when the input voltage is greater than the output voltage, and in boost mode for input voltages smaller than the output voltage. When the converter is operating in the transfer region, which is when the input voltage is in the range of the output voltage, there are two concepts for handling these conditions: either both the buck and boost stage are active at the same time, or the switching cycles alternate between the buck and boost stages, each usually running at half the regular switching frequency. The second concept can cause subharmonic noise at the output and the output-voltage precision can be a little bit less accurate compared to regular buck or boost operation, but the converter is much more efficient compared to the first concept.
The buck-boost topology has pulsed currents at the input and the output, as there is no LC filter pointing in either direction.
You can use the buck and boost power-stage calculations, respectively, for a buck-boost converter.
Buck-boost converters with two switches are designed for a power range between 50 W and 100 W (such as the LM5118), with synchronous rectification up to 400 W possible (as with the LM5175). Using synchronous rectifiers with the same current limits as for the uncombined buck and boost power stages is recommended.
Design the compensation network of a buck-boost converter for the boost stage, because the RHPZ is the limiting factor of the bandwidth of the regulator.
Part 4 discusses the features and drawbacks of the SEPIC and Zeta converter.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated