SLVAFJ9 March   2023 TPSF12C1 , TPSF12C1-Q1 , TPSF12C3 , TPSF12C3-Q1

 

  1.   Abstract
  2. Table of Contents
  3.   Trademarks
  4. Introduction
  5. EMI Frequency Ranges
  6. Passive EMI Filters for High-Power, Grid-Tied Applications
  7. Active EMI Filters
  8. Generalized AEF Circuits
  9. Selection of the CM Active Filter Circuit
  10. The Concept of Capacitive Amplification
  11. Practical AEF Implementations
  12. 10Practical Results
    1. 10.1 Low-Voltage Testing
    2. 10.2 High-Voltage Testing
  13. 11Summary
  14. 12References

The Concept of Capacitive Amplification

An AEF circuit for CM noise mitigation either amplifies the apparent inductance of a CM choke or the apparent capacitance of a Y-capacitor over the frequency range of interest. A VSCI AEF configured for CM attenuation uses an amplifier stage as a capacitive multiplier of the injection capacitor, CINJ. It is this higher value of active capacitance that supports lower values for the CM chokes to achieve a target attenuation.

Looking at Figure 7-1, Equation 1 shows that the injection capacitance is effectively multiplied by GAEF, the CM voltage gain from the power lines to the amplifier output:

Equation 1. v C I N J = 1 - G AEF ( f ) v AEF
i C I N J = C INJ d v C I N J d t = 1 - G AEF ( f )   C INJ d v AEF d t
C INJ,active ( f ) = 1 - G AEF ( f )   C INJ

Figure 8-1 shows a simulated plot of an injection network impedance when a FB-VSCI AEF circuit is enabled and disabled. The lower impedance above 2 kHz (and especially above 100 kHz) is caused by the capacitive amplification by the active circuit of a 4.7-nF injection capacitor and its associated damping network.

GUID-20230223-SS0I-G2QQ-NNR5-ZFGFNKMTMMMD-low.png Figure 8-1 Example of Inject Branch Impedance ZINJ With AEF Enabled vs. a Conventional Y-Capacitor, Showing the Boosted Equivalent Capacitance at Higher Frequencies by Active Feedback Action