This application brief highlights the workhorse of low-power isolated topologies: the flyback converter. The maximum achievable output power of this topology is typically in the range of 100 W. For output power above this level, using a forward topology can provide better efficiency. These topologies are the topic of the next installations in this series.
The flyback topology can step the input voltage up and down, generating an isolated output voltage that can be positive or negative. When switch Q1 is conducting, energy is stored in the air gap of the coupled inductor, often called a flyback transformer. The energy then transfers to the output when switch Q1 stops conducting. Figure 1-1 is a schematic of a nonsynchronous flyback converter.
Equation 1 calculates the duty cycle in continuous conduction mode (CCM).
Equation 2 calculates the maximum metal-oxide semiconductor field-effect transistor (MOSFET) stress.
where
The nonperfect coupling of the coupled inductor creates an additional voltage spike caused by the excess energy stored in the leakage inductance. Therefore, choose a voltage rating for Q1 that includes reasonable margin. Typically, a clamping circuit can reduce the voltage spike and needs to dissipate the excess energy. Generally, allow the overshoot to reach 50% of the reflected voltage to provide proper commutation of the stored energy to the output.
Equation 3 gives the maximum diode stress.
where
The flyback converter has pulsed currents at both ends of the converter because of how the converter transfers energy to the secondary side. This fact leads to rather high voltage ripple at both converter ends. For electromagnetic compatibility, additional input filtering can be necessary. If the converter needs to supply a very sensitive load, a second-stage filter at the output can help damp the output voltage ripple.
A flyback converter can be built by using a boost or general-purpose pulse-width modulation controller, because the converter only requires a low-side gate driver. For low output power, a boost converter integrated circuit (IC) (with integrated MOSFETs) can be a viable option.
In terms of dynamic behavior, an optocoupler in the isolated feedback path and right half-plane zero (RHPZ) are the primary limiting factors for the achievable regulation bandwidth of the flyback converter. If there is no optocoupler in the feedback path or the bandwidth is larger than the RHPZ frequency, the maximum achievable bandwidth is roughly one-fifth the RHPZ frequency. However, it is good practice opting for one-tenth the RHPZ frequency for the majority of designs to provide sufficient phase and gain margin. Equation 4 estimates the single RHPZ frequency of the transfer function of the flyback converter.
where
Figure 1-2 through Figure 1-7 show voltage and current waveforms in CCM for FET Q1, primary inductor Np, and diode D1 in a nonsynchronous flyback converter.
Low-power or low-output-current flyback converters are often designed to operate in discontinuous conduction mode (DCM) to minimize transformer size, weight, and cost. An additional benefit of this approach is that the RHPZ frequency moves to regions higher than 100 kHz, enabling higher regulation bandwidths than in CCM.
Equation 5 calculates the duty cycle in DCM.
where
Figure 1-8 through Figure 1-13 show voltage and current waveforms in DCM for FET Q1, primary inductor Np, and diode D1 in a nonsynchronous flyback converter.
Depending on the application, there are two different options to feed back the isolated output voltage to the controller on the primary side:
It is possible to generate multiple isolated outputs with a flyback by adding additional secondary windings to the coupled inductor. But if these multiple outputs are also isolated from each other, only one of them can be regulated properly. Choosing the winding with the highest current level for regulation is good practice for most designs to achieve satisfactory regulation results.
Using synchronous rectification for load currents over 2 A is advisable, especially when efficiency needs to be high or when external heat sinks need to be avoided. The synchronous rectifier can either be controlled from the primary side or use a self-driven concept, with the latter typically the more cost-effective option.