SLVAFM7 June 2024 TLC6983
Figure 2-8 shows seven common issues in high-density matrix LED displays. Some examples are shown in Figure 2-9 and Figure 2-10. The following session goes deeper into root cause analysis and TI designs of those typical LED display challenges from IC circuits and algorithm perspectives based on TI’s latest Common Cathode Matrix LED Display Driver, TLC6983 and TLC6984. Meanwhile, you can also refer to the application note The Common LED Display Challenges in Narrow Pixel Pitch Matrix LED Display for a rough overview about these issues.