SLVAFM7 June 2024 TLC6983
The main cause of downside ghosting is the buildup charge in the parasitic capacitance on OUTn when transitioning between scan lines, the charge on the parasitic capacitance discharges through the LED causing the LED to light up when the LED is not supposed to be.
Figure 3-3 lists the LED legend that is used in the following analysis.
Figure 3-4, Figure 3-5 and Figure 3-6 show the root cause analysis of downside ghosting with the simplified time-multiplexing LED driver structure for easier understanding.
So, in P1 operation, when only wanting to light up LED02, the driver turns ON SW0 and the current path is shown in red dotted line. At this moment, the yellow parasitic capacitor on channel OUT2 is charged.
During P1 operation, SW0 is ON, LED02 lights up.
Next, in P2 operation, when only wanting to light up LED11, the driver turns on SW1 and the current path is shown in red dotted line. And at this moment, the yellow parasitic capacitor on channel OUT1 is charged. However, LED12 is also slightly lit up even channel OUT2 is closed. Because the parasitic capacitor has been charged previously, and LED12 is lit up through the current path in blue dotted line. So, LED12 is called downside ghosting.
During P2 operation, SW1 is ON, LED11 lights up, and LED12 slightly lights up.
Similarly, in P3 operation, when only wanting to light up LED20,LED21 is also slightly lit up and LED22 is slightly lit up, through the current paths in blue and orange dotted line, respectively. The reason is the same as previously due to the channel parasitic capacitors.
The reason that LED21 and LED22 have different brightness is that the corresponding channel parasitic capacitors have different charges to light up the LED. Different quantities of charge flow through the LED to discharge the corresponding channel parasitic capacitor.
During P3 operation, SW2 is ON, LED20 lights up, LED21 slightly lights up, LED22 ever so slightly lights up.
So, how to solve this issue? We know that the downside ghosting is because of charges on channel parasitic capacitors. So, if we can remove these charges, then we can possibly to solve this issue.
As shown in Figure 3-7, TLC698x uses a pre-discharge circuit to pull all channels OUTn down to the set level (Vpd) during the line switch period to maintain LEDs in the next scan line are not lit up, thus eliminating downside ghosting.
Figure 3-8 shows the comparison demo with or without downside ghosting. You can see that the pre-discharge circuit works well. When enabled, we do not see ghosting anymore.