SLVAFQ5 December 2023 TPS51383 , TPS51385 , TPS51386
PRODUCTION DATA
The loop of the D-CAP3 converter is stable with the MLCC output capacitors network and the bandwidth is less than 1/3 switching frequency to make sure the loop is stable. When the hybrid output capacitor network is used, the loop stability is discussed in more detail.
Equation 9 shows the zero frequency minus the pole frequency, C1<C2, r1<r2, the result is less than 0. So the zero frequency is always less than the pole frequency, which can simplify the subsequent analysis and calculations. Since the ESR and capacitance of the MLCC is low, the zero ωz_C1 is typically located at a very high frequency and does not affect loop stability. The discussion focuses on the zero ωz_C2 and pole ωp_C2,, which is divided into two cases.
Case 1: When the ESR and capacitance of C2 is not large enough, and the zero ωz_C2 produced by the C2 is greater than ωcross and outside the bandwidth as shown in Figure 4-1. The ωz_C2 and ωp_C2 have little effect on the bandwidth and the bandwidth is less than 1/3×fsw.
The loop stable condition is ωz_C2 > ωcross, the crossover frequency can be calculated by:
The ωcross can be given by:
At the same time, the introduced C2 makes the double pole frequency ω0 become small and causes the crossing frequency to decrease as well. If the ωcross ≤ ωRI, the loop gain crosses 0 dB with -40-dB/decade slope, which results in the loop becoming unstable without enough phase margin. So, the loop stable condition is ωz_C2 > ωcross and ωcross > ωRI, which can be given by:
and
Case 2: when the ESR and capacitance is large enough, and ωz_C2 is pushed into the bandwidth as shown in Figure 4-2, ωz_C2 < ωcross. Since the gain curve passes through the zero ωz_C2, the slope of the gain curve becomes 0, which changes to -20dB/decade only when the slope encounters the pole ωp_C2. So, when the zero ωz_C2 enters within the bandwidth, the poles ωp_C2 must be inside the bandwidth, and the crossing frequency occurs after the ωp_C2. The zero and pole inside crossover frequency increases the bandwidth and can cause the loop to become unstable when the crossover frequency exceeds 1/3×fsw. To provide loop stabilization, the conditions that ωcross < 1/3×fsw and ωz_C2 < ωcross need to be met.
The crossover frequency can be calculated by:
The ωcross can be given by:
Summarizing the two previous conditions, the loop stable conditions can be given by:
or
If the ESR and capacitance of C2 is too large and the ωz_C2 is less than ωRI or ω0, the bandwidth increases more than case 2. This situation rarely occurs in the application design and the calculation of crossing frequency is more complex. Getting the crossover frequency through bench test is recommended because this method is simple and accurate. The ωcross calculation is not discussed more in-depth in this section. The calculation results are ideal and have deviation with the bench test results. Verifying the loops stability of the hybrid output capacitor network is recommended with the help of the bench loop test or simulation model. The suitable C2 can be selected based on the above principles and analysis method.