SLVAFU8 July 2024 TPSI2072-Q1 , TPSI2140-Q1 , TPSI3050 , TPSI3050-Q1 , TPSI3052 , TPSI3052-Q1 , TPSI3100 , TPSI3100-Q1
Electromechanical relays were first invented in the mid-19th century. These devices functioned as electrically operated switches by using a coil in combination with movable metal contacts. These devices can experience failure as the metal contacts experience wear and tear, such as welding shut. As a result, the device has a limited number of switching cycles before experiencing complete failure, thus limiting overall reliability.