SLVAFU8 July 2024 TPSI2072-Q1 , TPSI2140-Q1 , TPSI3050 , TPSI3050-Q1 , TPSI3052 , TPSI3052-Q1 , TPSI3100 , TPSI3100-Q1
A solid-state relay is an electronic switch that switches on or off when an external voltage is applied across the control terminals. Solid-state relays are typically used in the same applications as electromechanical relays; however, a key difference is that solid-state relays have no moving parts and can provide reliability benefits. Common examples of solid-state relays include optical or photo relays, or isolated switches and isolated switch drivers with capacitive or inductive isolation.