SLVAFV8 July   2024 TPS25751

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Introduction
  5. ADCINX Setting
  6. Unique Address Interface Protocol
  7. PTCH Mode to APP Mode
    1. 4.1 Step of PTCH Mode to APP Mode
    2. 4.2 Step of Generating Low Region Binary
  8. Dead Battery Configurations
  9. Interrupt Event, Mask, Clear for I2Ct IRQ
  10. GPIOx Function
  11. 4CC Command
  12. Summary
  13. 10References

Step of Generating Low Region Binary

Use USBCPB Application Customization Tool can easily generate the low region binary file. Select the system configuration and condition following the questionnaire. Then export the low region binary file shown as Figure 4-2. After generating the low region binary file, the host can see the content shown as Figure 4-3 for the bundle size and this is corresponding with the Section 4.1 step3.

 Setup for Generating the low
                    Regional Binary File Figure 4-2 Setup for Generating the low Regional Binary File
 Bundle Size Example Figure 4-3 Bundle Size Example