SLVAFV8 July 2024 TPS25751
Full name of 4CC is a four characters command. To use these 4CC commands, the ASCII command needs to be converted to hex and written to register 0x08. After the command is written, the command can be complete when register 0x08 clears. Then the user can check register 0x09 for the Output DataX to see if the task completed successfully. TPS25750 TRM shows the detailed DataX for task return code to see if the task is successfully written or not.