SLVAFW4 August   2024

 

  1.   1
  2.   2

This application brief highlights the forward converter. The output power range of this topology is typically between 100W and 250W. For output power above this level, a better design is possible using a push-pull or half-bridge topology for increased efficiency. These topologies are the topic of the next installations in this series.

Single-Switch Forward Converters

The single-switch forward topology can step the input voltage up and down, generating an isolated output voltage that can be positive or negative. When switch Q1 is conducting, energy is transferred from the primary to the secondary. Winding Nd and diode D3 provide a path to reset the transformer during demagnetization time. Diode D2 provides a freewheeling path when switch Q1 is not conducting. Figure 1 is a schematic of a nonsynchronous single-switch forward converter.


powerstage-designer Schematic of a Nonsynchronous
                    Single-Switch Forward Converter

Figure 1 Schematic of a Nonsynchronous Single-Switch Forward Converter

Equation 1 calculates the duty cycle in continuous conduction mode (CCM) as:

Equation 1. D = V O U T + V f V I N   ×   n s n p

where

  • VIN is the input voltage
  • VOUT is the output voltage
  • Vf is the diode forward voltage
  • np / ns is the turns ratio between the primary winding and the secondary winding

The maximum duty cycle is limited to 50% as the transformer needs sufficient time to be reset through the demagnetization winding.

Equation 2 calculates the maximum metal-oxide semiconductor field-effect transistor (MOSFET) stress as:

Equation 2. V Q 1 = 2 × V I N + V f

where

  • VIN is the input voltage
  • Vf is the diode forward voltage

The uncertain coupling of the transformer creates an additional voltage spike caused by the excess energy stored in the leakage inductance. Therefore, choose a voltage rating for Q1 that includes a reasonable margin.

Equation 3 gives the maximum rectifier diode stress as:

Equation 3. V D 1 = V I N + V f × n s n d - V f

where

  • VIN is the input voltage
  • Vf is the diode forward voltage
  • ns / nd is the turns ratio between the primary winding and the secondary winding

Equation 4 gives the maximum freewheeling diode stress as:

Equation 4. V D 2 = V I N × n s n p - V f

where

  • VIN is the input voltage
  • Vf is the diode forward voltage
  • ns / np is the turns ratio between the primary winding and the secondary winding

As the forward converter can be seen as a buck converter with a transformer, this converter family also has a continuous output current due to the output LC-filter and the freewheeling path through diode D2. Like a buck converter, the forward converter has a pulsed current at the input. This fact leads to rather high voltage ripple at the converter input. For electromagnetic compatibility, additional input filtering is likely necessary. If the converter needs to supply a very sensitive load, a second-stage filter at the output can help damp the output voltage ripple.

A single-switch forward converter can be built by using a boost or general-purpose pulse-width modulation (PWM) controller integrated circuit (IC), as this converter only requires a low-side gate driver.

In terms of dynamic behavior, an optocoupler in the isolated feedback path is the primary limiting factor of the achievable regulation bandwidth for the forward converter. If a high regulation bandwidth is required, the PWM controller can be placed on the secondary side of the converter.

Figure 2 through Figure 11 show voltage and current waveforms in CCM for FET Q1, primary transformer winding Np, rectifier diode D1, freewheeling diode D2, and inductor L1 in a nonsynchronous single-switch forward converter.


powerstage-designer Single-Switch Forward FET
                        Q1 Voltage Waveform in CCM

Figure 2 Single-Switch Forward FET Q1 Voltage Waveform in CCM

powerstage-designer Single-Switch Forward
                        Primary Transformer Winding Np Voltage Waveform in CCM

Figure 4 Single-Switch Forward Primary Transformer Winding Np Voltage Waveform in CCM

powerstage-designer Single-Switch Forward
                        Rectifier Diode D1 Voltage Waveform in CCM

Figure 6 Single-Switch Forward Rectifier Diode D1 Voltage Waveform in CCM

powerstage-designer Single-Switch Forward
                        Freewheeling Diode D2 Voltage Waveform in CCM

Figure 8 Single-Switch Forward Freewheeling Diode D2 Voltage Waveform in CCM

powerstage-designer Single-Switch Forward
                        Inductor L1 Voltage Waveform in CCM

Figure 10 Single-Switch Forward Inductor L1 Voltage Waveform in CCM

powerstage-designer Single-Switch Forward FET
                        Q1 Current Waveform in CCM

Figure 3 Single-Switch Forward FET Q1 Current Waveform in CCM

powerstage-designer Single-Switch Forward
                        Primary Transformer Winding Np Current Waveform in CCM

Figure 5 Single-Switch Forward Primary Transformer Winding Np Current Waveform in CCM

powerstage-designer Single-Switch Forward
                        Rectifier Diode D1 Current Waveform in CCM

Figure 7 Single-Switch Forward Rectifier Diode D1 Current Waveform in CCM

powerstage-designer Single-Switch Forward
                        Freewheeling Diode D2 Current Waveform in CCM

Figure 9 Single-Switch Forward Freewheeling Diode D2 Current Waveform in CCM

powerstage-designer Single-Switch Forward
                        Inductor L1 Current Waveform in CCM

Figure 11 Single-Switch Forward Inductor L1 Current Waveform in CCM

Two-Switch Forward Converters

For high-input voltage levels, a two-switch forward configuration can be leveraged, which enables the use of MOSFETs with a lower breakdown voltage and better performance parameters because the MOSFETs share the overall voltage stress. Figure 12 shows the schematic of a two-switch forward converter. The advantage of using two switches is that demagnetization can be achieved by having two clamping diodes to VIN and GND, allowing the removal of the demagnetization winding. To drive the two switches at the same time, with one of them being on the high-side, a half-bridge gate driver without interlock can be used in combination with a standard PWM controller.


powerstage-designer Schematic of a Nonsynchronous
                    Two-Switch Forward Converter

Figure 12 Schematic of a Nonsynchronous Two-Switch Forward Converter

Equation 5 calculates the maximum MOSFET stress in a two-switch forward converter as:

Equation 5. V Q 1 / 2 = V I N + V f

where

  • VIN is the input voltage
  • Vf is the diode forward voltage

This equation assumes that voltage stress is evenly distributed among the two MOSFETs. due to board and component parasitics as well as device parameter tolerances. Under certain circumstances the voltage stress is not distributed so evenly due to board and component parasitics as well as device parameter tolerances. Select a MOSFET breakdown voltage with sufficient margin to avoid fatal device failure.

Equation 6 gives the maximum rectifier diode stress as:

Equation 6. V D 1 = V I N + 2 × V f × n s n p - V f

where

  • VIN is the input voltage
  • Vf is the diode forward voltage
  • np / ns is the turns ratio between the primary winding and the secondary winding

Equation 1 and Equation 4 are also applicable for the two-switch forward converter.

Also, with two-switch configuration, the maximum duty cycle is limited to 50% as the transformer needs sufficient time to be reset through the demagnetization diodes.

Figure 13 through Figure 22 show voltage and current waveforms in CCM for FET Q1, primary transformer winding Np, rectifier diode D1, freewheeling diode D2, and inductor L1 in a nonsynchronous two-switch forward converter.


powerstage-designer Two-Switch Forward FET Q1
                        Voltage Waveform in CCM

Figure 13 Two-Switch Forward FET Q1 Voltage Waveform in CCM

powerstage-designer Two-Switch Forward Primary
                        Transformer Np Voltage Waveform in CCM

Figure 15 Two-Switch Forward Primary Transformer Np Voltage Waveform in CCM

powerstage-designer Two-Switch Forward
                        Rectifier Diode D1 Voltage Waveform in CCM

Figure 17 Two-Switch Forward Rectifier Diode D1 Voltage Waveform in CCM

powerstage-designer Two-Switch Forward
                        Freewheeling Diode D2 Voltage Waveform in CCM

Figure 19 Two-Switch Forward Freewheeling Diode D2 Voltage Waveform in CCM

powerstage-designer Two-Switch Forward
                        Inductor L1 Voltage Waveform in CCM

Figure 21 Two-Switch Forward Inductor L1 Voltage Waveform in CCM

powerstage-designer Two-Switch Forward FET Q1
                        Current Waveform in CCM

Figure 14 Two-Switch Forward FET Q1 Current Waveform in CCM

powerstage-designer Two-Switch Forward Primary
                        Transformer Np Current Waveform in CCM

Figure 16 Two-Switch Forward Primary Transformer Np Current Waveform in CCM

powerstage-designer Two-Switch Forward
                        Rectifier Diode D1 Current Waveform in CCM

Figure 18 Two-Switch Forward Rectifier Diode D1 Current Waveform in CCM

powerstage-designer Two-Switch Forward
                        Freewheeling Diode D2 Current Waveform in CCM

Figure 20 Two-Switch Forward Freewheeling Diode D2 Current Waveform in CCM

powerstage-designer Two-Switch Forward
                        Inductor L1 Current Waveform in CCM

Figure 22 Two-Switch Forward Inductor L1 Current Waveform in CCM

Active-Clamp Forward Converters

A third option to configure this topology is to use an active-clamp circuit on the primary side to recover energy from the leakage inductance of the transformer and feed the energy back to the input capacitor, boosting efficiency and enabling larger output power levels than the other two configurations. The active-clamp configuration also allows duty cycles larger than 50%. Figure 23 shows the schematic of a nonsynchronous active-clamp forward converter using an N-channel MOSFET for the clamping circuit.


powerstage-designer Schematic of a Nonsynchronous
                    Active-Clamp Forward Converter

Figure 23 Schematic of a Nonsynchronous Active-Clamp Forward Converter

Figure 24 through Figure 35 show voltage and current waveforms in CCM for FET Q1, FET Q2, primary transformer winding Np, rectifier diode D1, freewheeling diode D2, and inductor L1 in a nonsynchronous active-clamp forward converter.


powerstage-designer Active-Clamp Forward FET
                        Q1 Voltage Waveform in CCM

Figure 24 Active-Clamp Forward FET Q1 Voltage Waveform in CCM

powerstage-designer Active-Clamp Forward FET
                        Q2 Voltage Waveform in CCM

Figure 26 Active-Clamp Forward FET Q2 Voltage Waveform in CCM

powerstage-designer Active-Clamp Forward
                        Primary Transformer Np Voltage Waveform in CCM

Figure 28 Active-Clamp Forward Primary Transformer Np Voltage Waveform in CCM

powerstage-designer Active-Clamp Forward
                        Rectifier Diode D1 Voltage Waveform in CCM

Figure 30 Active-Clamp Forward Rectifier Diode D1 Voltage Waveform in CCM

powerstage-designer Active-Clamp Forward
                        Freewheeling Diode D2 Voltage Waveform in CCM

Figure 32 Active-Clamp Forward Freewheeling Diode D2 Voltage Waveform in CCM

powerstage-designer Active-Clamp Forward
                        Inductor L1 Voltage Waveform in CCM

Figure 34 Active-Clamp Forward Inductor L1 Voltage Waveform in CCM

powerstage-designer Active-Clamp Forward FET
                        Q1 Current Waveform in CCM

Figure 25 Active-Clamp Forward FET Q1 Current Waveform in CCM

powerstage-designer Active-Clamp Forward FET
                        Q2 Current Waveform in CCM

Figure 27 Active-Clamp Forward FET Q2 Current Waveform in CCM

powerstage-designer Active-Clamp Forward
                        Primary Transformer Np Current Waveform in CCM

Figure 29 Active-Clamp Forward Primary Transformer Np Current Waveform in CCM

powerstage-designer Active-Clamp Forward
                        Rectifier Diode D1 Current Waveform in CCM

Figure 31 Active-Clamp Forward Rectifier Diode D1 Current Waveform in CCM

powerstage-designer Active-Clamp Forward
                        Freewheeling Diode D2 Current Waveform in CCM

Figure 33 Active-Clamp Forward Freewheeling Diode D2 Current Waveform in CCM

powerstage-designer Active-Clamp Forward
                        Inductor L1 Current Waveform in CCM

Figure 35 Active-Clamp Forward Inductor L1 Current Waveform in CCM

Output Voltage Regulation Concepts

Depending on the application, there are two different options to feed back the isolated output voltage to the controller:

  • Secondary-side regulation (SSR), typically uses an optocoupler to transfer feedback information from the secondary to the primary side. Optocouplers have a limited bandwidth, which can affect the maximum achievable regulation bandwidth. Aging effects of the glass passivation in the optocoupler can be detrimental in certain applications. These applications then need to employ an optocoupler replacement, such as an isolated amplifier circuit or an opto-emulator.
  • Placing the controller on the secondary side can help achieve higher regulation bandwidths by eliminating the optocoupler in the feedback loop. However, an auxiliary power supply for start-up and short-circuit conditions is required to supply the PWM controller on the secondary. In addition, the MOSFETs on the primary side need to be driven with an isolated gate drive circuit, which can be implemented either with a dedicated isolated gate drive IC or with a discrete circuit leveraging a gate drive transformer and a non-isolated driver.

Using synchronous rectification for load currents over 3A is advisable, especially when efficiency needs to be high or when external heat sinks need to be avoided. The synchronous rectifier can either be controlled from the primary side or use a self-driven concept, with the latter typically the more cost-effective option.

Additional Resources