This report presents the effect of neutron displacement damage (NDD) on the TPS7H1111-SP device. The results show that all devices were fully functional and within production test limits after having been irradiated up to 1 × 1013 n/cm2[1-MeV(Si) equivalent]. A sample size of nine units were exposed per MIL-STD-883, Method 1017 for Neutron Irradiation, and two additional devices were used as control units. Electrical testing was performed at Texas Instruments before and after neutron irradiation using the production test program for TPS7H1111-SP.
All trademarks are the property of their respective owners.