SLVSAA4G June 2010 – February 2018 TPS65251
PRODUCTION DATA.
If a delayed start-up is required on any of the buck converters fit a ceramic capacitor to the ENx pins. The delay added is about 1.67 ms per nF connected to the pin. Note that the EN pins have a weak 1-µA pullup to the 3V3 rail.