SLVSB64I November 2011 – March 2018 TPS65217
PRODUCTION DATA.
The TPS65217x device has an analog multiplexer (mux) that provides access to critical system voltages. The voltages that can be measured by an ADC at the MUX_OUT pin are as follows:
In addition, one external input is available. The VBAT and VSYS voltages are divided by three (for example, MUX_OUT = VBAT / 3) to be compatible with the input-voltage range of the ADC that resides on the system-host side. The output of the MUX is buffered and can drive a maximum of 1-mA load current.