SLVSB64I November 2011 – March 2018 TPS65217
PRODUCTION DATA.
Functionality for this case is the same as for the shorted battery case. The only difference is that after the AC input is selected as the input, the power-path does not switch back to the USB input as AC input voltage decreases to less than 4.1 V.