SLVSCO0E June 2014 – October 2020 TPS22914 , TPS22915
PRODUCTION DATA
The VIN to VOUT voltage drop in the device is determined by the RON of the device and the load current. The RON of the device depends upon the VIN conditions of the device. Refer to the RON specification of the device in the Electrical Characteristics table of this datasheet. Once the RON of the device is determined based upon the VIN conditions, use Equation 1 to calculate the VIN to VOUT voltage drop.
where
An appropriate ILOAD must be chosen such that the IMAX specification of the device is not violated.