SLVSDC2C February 2016 – August 2021 TPS65981
PRODUCTION DATA
The TPS65981 first attempts to load application code from the low region of the attached flash memory. If any part of the read process yields invalid data, the TPS65981 will abort the low region read and attempt to read from the high region. If both regions contain invalid data the device carries out the Invalid Memory flow. Figure 9-56 shows the flow of the flash memory read.