SLVSDR3C may 2018 – may 2023 ADC12DL3200
PRODUCTION DATA
The analog inputs are protected against overdrive conditions by internal clamping diodes that are capable of sourcing or sinking input currents during overrange conditions; see the voltage and current limits in the Section 6.1 table. The overrange protection is also defined for a peak RF input power in the Section 6.1 table, which is frequency independent. Operation above the maximum conditions listed in the Section 6.3 table results in an increase in failure-in-time (FIT) rate, so the system must correct the overdrive condition as quickly as possible. Figure 7-1 shows the analog input protection diodes.