SLVSDZ5A February 2018 – January 2020 TPS2HB50-Q1
PRODUCTION DATA.
In this application, the TPS2HB50-Q1 must allow for the maximum 2.4-A current with margin but minimize the energy in the switch during a fault condition by minimizing the current limit. For this application, the best ILIM set point is approximately 4 A. Equation 7 allows you to calculate the RILIM value that is placed from the ILIMX pins to VBB. RILIM is calculated in kΩ.
Because this device is version A, the KCL value in the Specifications section is 40 A × kΩ.
For a ILIM of 4 A, the RILIM value should be set at approximately 10 kΩ.