SLVSEJ2A February 2018 – April 2018 TPSM84424
PRODUCTION DATA.
The EN pin provides electrical ON and OFF control for the TPSM84424. When the EN pin voltage is below the EN low threshold, the device is in shutdown mode. In shutdown mode the device is put into a low quiescent current state. The TPSM84424 also employs undervoltage lockout protection. If VIN is below the UVLO level, the output of the regulator turns off.