SLVSEK5A August 2018 – October 2018 TPS7B70-Q1
PRODUCTION DATA.
For LDO power supplies, especially high-voltage and high-current supplies, layout is an important step. If the layout is not carefully designed, the regulator cannot deliver enough output current because of thermal limitations. To improve the thermal performance of the device and maximize the current output at high ambient temperature, spread out the thermal pad as much as possible, and put enough thermal vias on the thermal pad. Figure 25 shows an example layout.