SLVSFE3C November 2020 – December 2021 TPS2661
PRODUCTION DATA
Select the ±Vs supplies for TPS2661x devices higher than absolute analog input voltage for ADC inputs.
TPS2661x devices have undervoltage and overvoltage protection on OUT pin and the internal FETs are turned
off if OUT pin has voltage higher than +Vs or lower than –Vs.
TPS2661x devices also have undervoltage protection on IN pin and the internal FETs are turned off if IN pin has a voltage lower than –Vs. See External Power Supply for using unipolar or bipolar supply with TPS2661x.