In this example the nominal load current is
100 mA, so the current limit can be set to 500 mA without disrupting normal
operation. Use Equation 4 to
calculate the resistor needed on the ILIM pin.
Equation 4. ILIM = 1.18 ×
(RILIM)–1.072
where
ILIM
= Typical current limit setting
RILIM = Resistor on the ILIM pin
Based on Equation 4,
a 2.21-kΩ resistor must be used on the ILIM pin to set a typical current
limit of 500 mA.