SLVSFX8A March 2021 – March 2022 TPS2521
PRODUCTION DATA
PIN | TYPE | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
EN/UVLO |
1 |
Analog Input | Active High Enable for the device. A Resistor Divider on this pin from input supply to GND can be used to adjust the undervoltage lockout threshold. Do not leave floating. Refer to Section 8.3.2 for details. |
OVCSEL |
2 |
Analog Input | Overvoltage clamp threshold select pin. Refer to Section 8.3.3 for details. |
PG |
3 |
Digital Output | Power Good indication. This pin is an Open Drain signal which is asserted High when the internal power path is fully turned ON and PGTH input exceeds a certain threshold. Refer to Section 8.3.9 for more details. |
PGTH |
4 |
Analog Input | Power Good Threshold. Refer to Section 8.3.9 for more details. |
IN |
5 |
Power |
Power input |
OUT |
6 |
Power |
Power output |
DVDT |
7 |
Analog Output | A capacitor from this pin to GND sets the output turn on slew rate. Leave this pin floating for the fastest turn on slew rate. Refer to Section 8.3.4.1 for details. |
GND |
8 |
Ground |
This pin is the ground reference for all internal circuits and must be connected to system GND. |
ILM |
9 |
Analog Output | This pin is a dual function pin used to limit and monitor the output current. An external resistor from this pin to GND sets the output current limit threshold during start-up as well as steady state. The pin voltage can also be used as analog output load current monitor signal. Do not leave floating. Refer to Section 8.3.4.2 for more details. |
ITIMER |
10 |
Analog Output | A capacitor from this pin to GND sets the overcurrent blanking interval during which the output current can temporarily exceed set current limit (but lower than fast-trip threshold) before the device overcurrent response takes action. Leave this pin open for fastest response to overcurrent events. Refer to Section 8.3.4.2 for more details. |