SLVSGC1B December 2021 – August 2024 TPS63901
PRODUCTION DATA
The device has a built-in short circuit protection function to limit the current through Q1. The maximum current that flows is limited by the peak current limit. The output voltage decreases if the load is higher than the peak current limit. If the output voltage falls below 1.25 typically, the short circuit protection is activated. With short circuit protection activated, the input current is limited to 26 mA on average.
The device automatically restarts to normal operation after the short condition is removed.